Enabling Efficient Edge AI with DEEPX NPUs and the Avnet Silica Ecosystem | Avnet Silica

Enabling Efficient Edge AI with DEEPX NPUs and the Avnet Silica Ecosystem | Avnet Silica

Enabling Efficient Edge AI with DEEPX NPUs and the Avnet Silica Ecosystem

Michaël Uyttersprot, Market Segment Manager Artificial Intelligence and Vision
DEEPX webinar image teaser shows DEEPX AI modules

Artificial intelligence is rapidly moving from the cloud to the edge. From autonomous robots navigating complex environments to smart cameras inspecting production lines, many applications now require AI to run directly on embedded devices, where power, latency, and thermal constraints are critical. However, deploying high-performance AI at-the-edge has traditionally required large Graphics Processing Units (GPUs) or power-hungry processors, making it difficult to build compact, energy-efficient systems.

DEEPX is rewriting the rule book. Its family of ultra-efficient Neural Processing Units (NPUs) enables powerful AI inference directly on edge devices while consuming only a fraction of the power of conventional AI accelerators. Together with Avnet Silica’s hardware platforms, engineering expertise, and partner ecosystem, developers and system designers can rapidly build and deploy scalable edge AI solutions.

 

A brief overview of DEEPX NPUs

DEEPX has developed a range of dedicated AI accelerators designed specifically for on-device inference at the edge. These NPUs are optimised to deliver high performance while maintaining extremely low power consumption and minimal thermal output.

For example, the DX-M1 NPU can perform advanced AI tasks such as video analytics, object detection, and sensor data processing while consuming only a few watts of power. To visually demonstrate the efficiency of the DEEPX NPU is the so-called ‘butter-proof’ benchmark test (Figure 1).

In this test, a piece of butter is placed directly on the NPU while it runs demanding AI workloads such as video analysis. Because butter melts at roughly 30 °C to 36 °C, it provides a simple visual indicator of how much heat the chip generates. During the demonstration, the butter does not melt, illustrating the DEEPX chip's extremely low heat output and power consumption.

The test highlights one of the key advantages of the DEEPX architecture: high AI performance without the need for large heatsinks or active cooling, making it ideal for embedded and edge systems where space and thermal budgets are limited.
 

DEEPX NPU butter proof testFigure 1: Benchmarking the DEEPX NPU using the ‘butter-proof’ test illustrates its extremely low heat output and power consumption

By processing AI workloads locally, edge devices gain several advantages:

 

  • Ultra-low latency for real-time decision making
  • Reduced bandwidth usage by avoiding cloud data transfers
  • Improved privacy and security by keeping data local
  • Higher reliability even in environments with limited connectivity

This architecture opens the door to a new generation of intelligent edge devices across industries, including robotics, manufacturing, medical, security, and smart infrastructure.

 

Edge AI in action

Since the launch of engineering samples in 2023, DEEPX has experienced rapid growth in market interest, engaging with over 350 global companies for testing, and now has over 50 customer projects in full production.

Hyundai

Working with Hyundai in Korea, the company replaced the GPU - needed to run two AI models concurrently - with its DX-M1 connected to a general-purpose ARM processor. In this smart mobility application, the commercial delivery robots are used in urban areas for last-mile food and package deliveries.

The robot runs facial recognition models on its camera (Figure 2). Upon delivery, it matches the photo of the customer taken from the smartphone used at the time of purchase. The robot can then automatically verify the recipient and open the hatch of the appropriate storage compartment to release the food or goods.

In parallel to the facial recognition models, another camera runs a positional awareness model to determine the position of the recipient’s feet – you do not want the robot to run over their toes. Using the DX-M1 device running at less than 5 W instead of a 20 W, 30 W or 40 W GPU-based application reduces the number of charge cycles significantly.

DEEPX NPU commercial delivery robotFigure 2: Commercial delivery robot using the DEEPX DX-M1 – finished verification and ready for mass production

 

Ultralytics

DEEPX has also supported various types of factory automation applications. Working in close collaboration with Ultralytics, the company behind the YOLO object detection models, two particular use cases stand out.

The first is for defect detection. As shown on the right in Figure 3, AI-enabled cameras are used to detect scratches and dents on the product’s casing. It also runs object character recognition (OCR) on the letters on the barcode to identify the defective product. The right-hand image illustrates how Ultralytics used the DX-M1 in combination with an x86 host, to count anything from tins to bottles. Neither of these application types is unique, but both solutions can run complex models on multiple cameras at below 5 W and at a lower cost.

DEEPX NPU automated quality controlFigure 3: Automated quality control on a fast-moving production line

Accelerating Edge AI with the Avnet Silica ecosystem

While powerful silicon is essential, bringing Edge AI products to market requires far more than a processor. This is where Avnet Silica plays a critical role. Working closely with DEEPX, Avnet Silica provides a complete ecosystem that helps designers move from concept to production faster.

This ecosystem includes:

  • Processor partnerships: Compatibility with leading application processors, using the PCIe interface, from vendors such as AMD, NXP, Renesas, TRIA, Microchip, STMicroelectronics, and Qualcomm, enables flexible system architectures.
  • Hardware platforms: Industrial PCs, embedded modules, and edge computing platforms that integrate DEEPX NPUs like Advantech, avalue, ASRock, ASUS IoT, Engicam, GigaIPC, Kontron, and MSI.
  • Software and OS: Avnet Silica’s technical teams help customers design, integrate, and optimise AI systems tailored to their applications with suppliers including Ubuntu Linux, Yocto Linux, and Microsoft Windows 11 IOT.
  • AI ecosystem partners: From robotics platforms to industrial automation systems, the broader partner network helps accelerate real-world deployment.

Together, DEEPX and Avnet Silica provide a pathway for companies to adopt edge AI without building the entire infrastructure themselves.

 

Enabling developers with the DEEPX SDK

A powerful chip also requires accessible tools for developers. The DEEPX software development kit (SDK) provides the environment needed to deploy Edge AI models efficiently on DEEPX hardware (Figure 4).

The SDK supports:

  • AI model optimisation and compilation
  • Deployment of vision AI and deep learning models
  • Integration with common AI frameworks
  • Performance tuning for edge environments

Developers can adapt existing AI models for efficient inference on DEEPX NPUs, enabling rapid prototyping and production deployment. Combined with Avnet Silica’s hardware platforms and engineering expertise, the SDK helps transform AI concepts into scalable edge solutions.

DEEPX NPU overview with AI model - DXNN Full Stack ArchitectureFigure 4: DEEPX SDK overview with AI model compile and runtime environments

Turning Edge AI innovation into reality

Edge AI is transforming industries, from autonomous robotics to smart manufacturing, by enabling devices to process data and make real-time decisions. With its highly efficient NPUs, DEEPX enables the execution of powerful AI workloads directly on embedded systems without the power and thermal limitations of conventional accelerators.

Through its collaboration with DEEPX, Avnet Silica provides the hardware platforms, ecosystem partnerships, and engineering support needed to bring these solutions to market faster. The end goal is to help companies unlock the full potential of Edge AI.

Ready to bring AI to your edge devices? Avnet Silica can help you explore the DEEPX platform, integrate the technology into your designs, and accelerate your transition from prototype to production. Contact Avnet Silica to learn how the DEEPX ecosystem can power your next generation of Edge AI solutions.

 

Frequently asked DEEPX/NPU questions

Question Answer
What is the difference between TOPS and equivalent TOPS?

TOPS (Trillion Operations Per Second) is a theoretical measure of a processor's peak mathematical capacity. However, raw TOPS can be misleading if the hardware suffers from memory bottlenecks or inefficient data handling.

eTOPS (equivalent TOPS) measures effective throughput—the actual work delivered on real-world AI models. DEEPX achieves high eTOPS by using architectural innovations like weight compression, sparsity support (skipping zero-value calculations), and near-memory computing. This allows a DEEPX NPU with lower power consumption to match or exceed the frames-per-second (FPS) of a high-wattage GPU with a higher "paper" TOPS rating. Essentially, eTOPS represents "useful" AI performance rather than just raw, idle cycles.

Why are FPS/TOP and FPS/W important when comparing GPUs and NPUs?

When comparing AI processors, especially GPUs and dedicated NPUs used in vision systems, two additional metrics are very useful:

  • A higher frames-per-second per TOP (FPS/TOP) equates to better architectural efficiency, lower overhead when executing neural networks, and higher practical performance for the same compute rating.
  • Frames-per-second per Watt (FPS/W) is particularly important for edge applications because it directly affects battery life, thermal design requirements, system reliability, and operating costs.
Why are dedicated NPUs becoming more popular for edge AI? While GPUs are extremely powerful and flexible, they were originally designed for graphics workloads and large-scale compute environments. Dedicated NPUs are designed specifically for neural network inference, which allows them to deliver higher performance per watt, lower thermal output, smaller silicon footprints, and optimised execution of AI models.
How easy is it to port existing AI models to DEEPX NPUs? Porting existing AI models to DEEPX NPUs is designed to be relatively straightforward, especially if the model was originally trained using common deep learning frameworks. The key reason is that DEEPX uses the ONNX (Open Neural Network Exchange) format as its primary model input. ONNX serves as a universal model representation, enabling neural networks trained in frameworks such as PyTorch, TensorFlow, or scikit-learn to be exported to a common format for deployment across different hardware platforms.

 

On Demand Webinar: Deploying Edge AI at GPU-Level Performance with DEEPX

On demand webinar image for DEEPX AI webinar shows DEEPX logo with an AI chip and play button overlay

Join Avnet Silica and DEEPX for an exclusive one-hour webinar introducing cutting-edge AI inference acceleration technology now available in Europe. As the demand for edge AI continues to grow, traditional GPU solutions often fall short in power efficiency and thermal constraints. DEEPX addresses this critical gap with purpose-built edge-first AI processors that deliver exceptional performance per watt while maintaining high-precision inference.

Over 240 attendees joined us for the live webinar, making it one of our most-attended online events to date. Catch up below!

WATCH ON DEMAND

 

Episode 83: 100 TOPS, Zero Production: Why Edge AI Projects Die Between Demo and Deployment

Edge AI promised intelligence everywhere. The reality? Most projects die between proof of concept and production. In this episode, Amir Sherman from DEEPX and Michaël Uyttersprot from Avnet Silica reveal why moving AI from comfortable development kits to demanding industrial environments isn't just difficult. It's a maze of incompatible metrics, hidden power costs, and integration nightmares that catch companies off guard.

We discuss why TOPS ratings mislead engineers, how ChatGPT triggered a wave of failed internal deployments, and what it takes to run vision AI in factories, delivery robots, and smart cities where five-watt power budgets matter more than marketing specifications.

From Hyundai's factory robots to Baidu's Chinese character recognition systems, Amir and Michaël share real deployments that work, and explain the 50 years of embedded experience that AI code generators cannot replace. If you've wondered why edge AI keeps hitting walls nobody discusses in vendor presentations, this conversation delivers the answers.

SEE FULL OVERVIEW

SEE DEEPX OVERVIEW

About Author

Michaël Uyttersprot, Market Segment Manager Artificial Intelligence and Vision
Michaël Uyttersprot

Michaël Uyttersprot is Avnet Silica's Market Segment Manager for Artificial Intelligence, Machine Le...

Helpful Links

Enabling Efficient Edge AI with DEEPX NPUs and the Avnet Silica Ecosystem | Avnet Silica

Hardware Solutions for AI

Understanding the unique opportunities and hardware challenges across different deployment tiers is essential for designing impactful AI systems that meet the demands of modern applications.

Avnet Silica QCS6490 Vision-AI Development Kit

Enabling Efficient Edge AI with DEEPX NPUs and the Avnet Silica Ecosystem | Avnet Silica

Related Articles
Trendliner cover - Q4 2026
Semiconductor Market Pulse: Five Insights for Q4 2026
By Thomas Foj   -   November 13, 2026
Exploring the current semiconductor market shifts, technological trends, and supply-chain signals influencing Q3 2026.
Smart factory robotics in a car manufacturing plant
From Robots to Production Lines: Why NPUs Are Emerging as the New Standard for Real-Time Industrial AI
By Michaël Uyttersprot   -   September 28, 2026
Industrial robotics and smart factories are increasingly being designed as unified cyber-physical systems.

Enabling Efficient Edge AI with DEEPX NPUs and the Avnet Silica Ecosystem | Avnet Silica

Related Events
STMicroelectronics Tech Innovation Day
STMicroelectronics Tech Innovation Day
Date: December 1, 2026
Location: Poland, Gdansk
A group of people are listening the seminar
AMD Agentic AI tools and high-speed IO workshop
Date: November 30, 2026
Location: Germany, Hamburg

Related Designs Menu