Why Performance per Watt Is Becoming the Key Metric in Edge AI | Avnet Silica

Why Performance per Watt Is Becoming the Key Metric in Edge AI | Avnet Silica

Why Performance per Watt Is Becoming the Key Metric in Edge AI

Michaël Uyttersprot, Market Segment Manager Artificial Intelligence and Vision
Magnifying glass showing bar graph statistics

For decades, improvements in computing have been measured in terms of peak capability—more Trillion Operations Per Second (TOPS), higher throughput, faster execution. That model still holds in data centres, where power and cooling can scale alongside compute demand. At the edge, however, the situation is different.

Edge systems operate within defined limits. Power is often capped by Power over Ethernet (PoE) budgets or battery capacity. Thermal headroom is restricted by fanless designs or sealed enclosures. In many deployments, systems must run continuously for extended periods without intervention, making reliability a primary design concern alongside performance.

Under these conditions, raw compute capability is only one part of the design equation. The more important question is how much useful work can be sustained within those fixed constraints.

 

The realities of edge deployment

Edge AI deployments must often operate in highly unforgiving environments. Industrial systems may be exposed to elevated ambient temperatures, dust, or vibration. Deployments including smart cameras, industrial PCs, and embedded systems are often located outdoors, where conditions vary widely. Mobile platforms such as robots must operate within strict energy budgets while maintaining consistent behaviour over long periods.

These constraints are not theoretical; they directly affect whether a system can be deployed and how it performs in operation. A system that exceeds its thermal limits will begin to throttle and, in extreme cases, fail, while a platform that draws too much power may require active cooling, larger enclosures, or higher-capacity power supplies, making it impractical for many edge deployments. In both cases, the result is reduced performance consistency —often expressed as increased or unpredictable latency, which can affect safety, coordination, or product quality in real-time applications.

As a result, system designers are working within a narrow operating envelope:

  • Latency requirements are often below 100 ms for real-time perception and control
  • Reliability targets approaching 99.999 % uptime in production environments
  • Power budgets typically within 5–20 W, depending on PoE, battery, or embedded constraints
  • Thermal limits that favour passive cooling, with junction temperatures needing to remain below 85 °C

In practice, the challenge is to sustain performance over time within these limits, rather than achieve short bursts of peak output.

 

Why peak compute is an incomplete measure

A processor capable of high peak performance may still be poorly suited to edge deployment if that performance depends on power budgets, cooling capacity, or thermal headroom that the target system cannot provide. In practice, the relevant question is not how fast a processor can run under ideal conditions, but whether that performance can be sustained reliably in its intended operating environment.

This is particularly true when:

  • power consumption exceeds system limits
  • active cooling or large thermal solutions are required
  • performance cannot be sustained under real operating conditions

Systems designed around peak compute often encounter secondary challenges in deployment. Thermal management becomes more complex, introducing additional components and potential failure points. Energy consumption increases operating costs over time. In some cases, workloads must be offloaded to the cloud, introducing latency and dependency on network connectivity.

These factors mean that peak performance alone does not determine whether a solution is viable in its intended operating environment.

 

Defining performance in terms of efficiency

To evaluate edge AI platforms effectively, performance must be considered alongside the resources required to achieve it. This is where performance per watt becomes a useful metric.

At a basic level, performance per watt reflects how efficiently a system converts electrical power into useful computational output. More importantly, it provides a practical way to compare architectures against SWaP-C (size, weight, power, and cost), the core constraints that determine whether an edge AI system is viable in real-world deployment.

A system with higher performance per watt can:

  • Deliver consistent throughput within a fixed power budget
  • Operate within tighter thermal limits without throttling
  • Reduce or eliminate the need for active cooling
  • Enable deployment in environments where power and space are limited

In practice, efficiency often determines whether a system can be deployed at all.

 

System-level implications of efficiency

Focusing on performance per watt has implications beyond the processor itself, shaping the design and behaviour of the entire system. Lower power consumption reduces heat generation, which in turn simplifies thermal management. Fanless designs become more practical, improving reliability by removing moving parts, which are often a primary point of failure in industrial hardware. Lower thermal stress can also improve mean time between failures (MTBF), extending product life and reducing the need for costly on-site maintenance. Systems can be sealed against dust and moisture, making them suitable for harsher environments. Consistent thermal behaviour also leads to more predictable performance. When a processor operates within its thermal limits, latency remains stable and deterministic—an important requirement for real-time control systems and safety-critical applications. Energy efficiency also affects long-term cost. Systems that consume less power require less cooling and incur lower operating expenses over their lifetime. In large-scale deployments, these differences accumulate quickly.

These factors link efficiency directly to reliability, scalability, and total cost of ownership, making it a core consideration in system design.

DEEPX Lower-power AI architectureFigure 1: Lower-power AI architectures reduce thermal stress, enabling fanless edge designs with improved reliability, longer MTBF, and lower maintenance requirements.

 

Applying the metric in practice

These principles are now reflected in emerging edge AI architectures, where benchmark data increasingly highlights performance per watt as a differentiating factor. For example, YOLOv7 comparisons reported in DEEPX’s Lower Power, Heat, and Bill analysis, figure 2, — which examines performance under real-world edge constraints — show a significant gap between architectures optimised for efficiency and those designed primarily for peak compute. Performance figures of around 40 frames per second per watt—a measure of how much inference performance is delivered for each watt of power—have been demonstrated, compared with approximately 2 frames per second per watt for traditional general-purpose GPU or high-power CPU architectures.

 

  DX-M1 Competitor A Competitor B GPGPU
Performance
(FPS/W)
40 20 23 2
Processing
Efficiency
(FPS/TOPS)
8 4 0.8 1.3
Power
Consumption
Avg. 2~3 W Avg. 5 W Avg. 4~8 W Avg. 40 W

Figure 2: YOLOv7 benchmark comparison showing the performance-per-watt advantage of AI-optimised NPU architectures over traditional GPU and CPU-based approaches in edge inference workloads.

 

Alongside this improvement in efficiency, power consumption can be reduced from tens of watts to only a few watts per device, reflecting architectures that are designed specifically for AI inference rather than general-purpose compute. Operating within such a range allows systems to remain within thermal limits without active cooling, even under sustained workloads. Lower power draw reduces thermal stress and helps maintain stable operation over extended periods, making performance more predictable, particularly in environments where conditions vary.

These emerging AI-optimised architectures enable AI processing to be integrated into a wider range of edge systems, including deployments where power, cooling, and space are tightly constrained.

 

Designing for constrained environments

As edge AI continues to expand into industrial systems, robotics, and distributed infrastructure, the criteria for evaluating performance are becoming more closely aligned with deployment realities. Design decisions are increasingly driven by questions such as:

  • Can the system operate within a fixed power budget?
  • Will performance remain stable over time and temperature?
  • Can the design be simplified to improve reliability and reduce maintenance?

In many cases, these questions carry more weight than absolute compute capability. However, bridging the gap between theoretical efficiency and a ruggedised, deployed system requires a collaborative ecosystem. Through its partnership with DEEPX, Avnet Silica helps customers navigate these trade-offs, providing the technical expertise to align AI-optimised architectures like the DX-M1, figure 3, with real-world power, thermal, and integration constraints. This keeps efficiency at the centre of architectural decisions, ensuring a practical path to reliable edge deployment.

Top view of DEEPX DX-M1 moduleFigure 3: The DEEPX DX-M1 module, illustrating the class of AI-optimised accelerators that Avnet Silica helps customers integrate into production-ready edge systems.

 

Conclusion

Edge AI systems are defined by the environments in which they operate. Power, thermal limits, and reliability requirements shape what is achievable, and these factors cannot be treated as secondary considerations.

Within these constraints, performance must be measured differently. Efficiency—expressed as performance per watt—provides a more meaningful indication of how a system will behave in practice, capturing both achievable throughput and the ability to sustain it over time.

As edge deployments scale and diversify, this perspective is becoming more relevant. Systems are being designed to operate within fixed limits, and success depends on making effective use of those available resources.

Performance per watt is therefore a practical way to assess whether an AI system can be deployed and operated reliably at the edge.

 

On Demand Webinar: Deploying Edge AI at GPU-Level Performance with DEEPX

On demand webinar image for DEEPX AI webinar shows DEEPX logo with an AI chip and play button overlay

Join Avnet Silica and DEEPX for an exclusive one-hour webinar introducing cutting-edge AI inference acceleration technology now available in Europe. As the demand for edge AI continues to grow, traditional GPU solutions often fall short in power efficiency and thermal constraints. DEEPX addresses this critical gap with purpose-built edge-first AI processors that deliver exceptional performance per watt while maintaining high-precision inference.

Over 240 attendees joined us for the live webinar, making it one of our most-attended online events to date. Catch up below!

WATCH ON DEMAND

 

Episode 83: 100 TOPS, Zero Production: Why Edge AI Projects Die Between Demo and Deployment

Edge AI promised intelligence everywhere. The reality? Most projects die between proof of concept and production. In this episode, Amir Sherman from DEEPX and Michaël Uyttersprot from Avnet Silica reveal why moving AI from comfortable development kits to demanding industrial environments isn't just difficult. It's a maze of incompatible metrics, hidden power costs, and integration nightmares that catch companies off guard.

We discuss why TOPS ratings mislead engineers, how ChatGPT triggered a wave of failed internal deployments, and what it takes to run vision AI in factories, delivery robots, and smart cities where five-watt power budgets matter more than marketing specifications.

From Hyundai's factory robots to Baidu's Chinese character recognition systems, Amir and Michaël share real deployments that work, and explain the 50 years of embedded experience that AI code generators cannot replace. If you've wondered why edge AI keeps hitting walls nobody discusses in vendor presentations, this conversation delivers the answers.

SEE FULL OVERVIEW

SEE DEEPX OVERVIEW

About Author

Michaël Uyttersprot, Market Segment Manager Artificial Intelligence and Vision
Michaël Uyttersprot

Michaël Uyttersprot is Avnet Silica's Market Segment Manager for Artificial Intelligence, Machine Le...

Helpful Links

Why Performance per Watt Is Becoming the Key Metric in Edge AI | Avnet Silica

Hardware Solutions for AI

Understanding the unique opportunities and hardware challenges across different deployment tiers is essential for designing impactful AI systems that meet the demands of modern applications.

Avnet Silica QCS6490 Vision-AI Development Kit

Why Performance per Watt Is Becoming the Key Metric in Edge AI | Avnet Silica

Related Articles
Trendliner cover - Q4 2026
Semiconductor Market Pulse: Five Insights for Q4 2026
By Thomas Foj   -   November 13, 2026
Exploring the current semiconductor market shifts, technological trends, and supply-chain signals influencing Q3 2026.
Smart factory robotics in a car manufacturing plant
From Robots to Production Lines: Why NPUs Are Emerging as the New Standard for Real-Time Industrial AI
By Michaël Uyttersprot   -   September 28, 2026
Industrial robotics and smart factories are increasingly being designed as unified cyber-physical systems.

Why Performance per Watt Is Becoming the Key Metric in Edge AI | Avnet Silica

Related Events
STMicroelectronics Tech Innovation Day
STMicroelectronics Tech Innovation Day
Date: December 1, 2026
Location: Poland, Gdansk
A group of people are listening the seminar
AMD Agentic AI tools and high-speed IO workshop
Date: November 30, 2026
Location: Germany, Hamburg

Related Designs Menu