Custom Meta Tags

Hero Banner

Sub Navigation

Title and intro (LC)

AI Latency Targets Define the Hardware Long Before Deployment: How AI Latency Requirements Shape Hardware Selection

Artificial intelligence (AI) is moving beyond digital environments into physical systems where models must interact with real-world processes in real time. This transition is accelerating, with deployments across manufacturing and logistics projected to exceed 400,000 systems by 2030, representing a 3,500% expansion from 2026[1].

However, unlike cloud-based or offline AI workloads, these systems operate under direct environmental constraints. Decisions are no longer abstract outputs, but actions that affect machines, processes, and safety-critical operations.

CONTACT OUR AI EXPERTS

Intro cont (MM)

In these environments, response time is not simply a performance metric; it becomes a defining system requirement. For engineers, this changes the starting point. Once latency targets and determinism requirements are defined, some hardware options are no longer viable, regardless of their theoretical compute capability.

As AI continues to move into physical systems, latency is no longer something that can be optimised late in the design process. It becomes an architectural constraint that shapes hardware selection and system design long before deployment.

When Latency Defines Real-Time AI Systems

Physical AI’s early adoption is concentrating in high-value sectors such as automotive, industrial infrastructure, and robotics, where real-time decision-making directly affects performance, safety, and efficiency. By 2030, these systems are expected to contribute to a global market of approximately €430 billion[2], with automotive alone accounting for around €171 billion, reflecting both scale and complexity of deployment.

In automotive systems, AI can enable vehicles to move beyond rule-based assistance toward systems that interpret complex, dynamic environments in real time, supporting higher levels of autonomy and more advanced driver assistance systems (ADAS). However, enabling this capability requires continuous processing of high-bandwidth sensor data from cameras, radar, and LiDAR, as well as real-time decision-making and actuation. As a result, deterministic latency becomes a fundamental requirement, constraining how and where data is processed, and ultimately the hardware architecture that supports it.

Conceptual illustration of data streams passing through a narrow bottleneck, representing memory bandwidth limitations and latency challenges in edge AI systems
As AI continues to move into physical systems, latency is no longer something that can be optimised late in the design process. It becomes an architectural constraint that shapes hardware selection and system design long before deployment.

Main body (LC)

In industrial environments, AI enables systems to move from retrospective analysis toward real-time monitoring and control, embedding intelligence directly within production processes. This includes applications such as in-line quality inspection, adaptive process control, and predictive maintenance, where equipment health is continuously monitored to detect faults before failure. In these systems, the potential impact of AI is linked to operational output and efficiency, but its effectiveness depends on how quickly it can respond to changing conditions.

AI is a cornerstone in the emergence of next-generation robotic systems, enabling a shift from pre-programmed behaviour toward more adaptive and autonomous operation. By combining perception, decision-making, and actuation in continuous loops, AI supports applications such as autonomous navigation, dynamic object handling, and collaborative robotics, where machines must operate safely alongside humans. However, in these environments, the unstructured and variable nature of the operating conditions means that complex decisions and sensor fusion are not only required but must be executed within tightly constrained timeframes.

Other sectors are also beginning to adopt similar approaches. In aerospace, low-latency processing supports autonomous and multi-agent systems operating in time-critical environments. In healthcare, robotic assistance and monitoring systems benefit from more immediate feedback and control, although regulatory and integration challenges remain. Across consumer and entertainment applications, real-time interaction is enabling more responsive and immersive systems.

Latency vs Throughput in AI Systems: Defining the Constraint

In many AI systems, their ultimate capability is often associated with compute performance and throughput, but in real-time and physically interactive applications, these are not always the limiting factors. Instead, the ability to respond quickly and predictably becomes the primary constraint.

Latency is the time between an input and the corresponding system response, while throughput is the amount of data processed per unit time. Systems optimised for throughput rely on parallelism and batching, grouping data or inference requests together to maximise utilisation. While efficient, this can introduce delay, as data may need to be accumulated before processing begins.

By contrast, latency-sensitive applications prioritise immediacy, processing data as it is received rather than waiting for batch accumulation. This is often achieved through streaming architectures, where data flows continuously through the system. In these environments, the requirement is not simply low latency but deterministic latency, in which response times are predictable and bounded.

As a result, systems optimised for throughput prioritise efficiency and scale, while those designed for real-time operation prioritise predictable execution and data flow, fundamentally shaping how workloads must be executed from the outset.

How Latency Targets Shape System Architecture

Once latency targets are defined, they begin to shape system architecture at multiple levels, from the processing model through the data movement, memory hierarchy, interfaces, and platform selection.

At the highest level, latency requirements influence how workloads are executed. Systems optimised for throughput often rely on batch-based execution, where data or inference requests are grouped to maximise utilisation, an approach well aligned to many GPU-based workloads. Latency-optimised systems, by contrast, tend to favour streaming or pipelined execution, where data is processed as it arrives and unnecessary queueing is reduced.

AI ML Overview (GBL)

Technology

Artificial Intelligence Overview

Head over to our Artificial Intelligence overview page for more AI articles, applications and resources.

Artificial Intelligence connections

Knowledge Library (GBLS)

See the AI Knowledge Library

Head over to the AI Knowledge Library to see all of our AI and ML resources in one place. Explore articles, webinars, podcasts and more.

SEE KNOWLEDGE LIBRARY

Main body and conclusion (LC)

For engineers deploying real-time applications, latency must be considered from end-to-end. Delays can be introduced before the model even runs, through sensor interfaces, analogue-to-digital conversion, image or signal pre-processing, memory transfers, buffering, protocol overhead, and communication between subsystems. A model may meet its latency target in isolation but still fail at the system level if data must repeatedly move among sensors, external memory, processors, and control logic before an action can be taken.

This is why many of the latest semiconductor platforms designed for edge and real-time AI now integrate more of the data path into hardware. System-on-chip (SoC) devices may combine camera or audio interfaces, image signal processors (ISPs), digital signal processors (DSPs), neural processing units (NPUs), direct memory access (DMA) engines, local static random-access memory (SRAM), and real-time control cores to reduce data movement and keep inference close to the input.

FPGAs and adaptive SoCs are often used in latency-sensitive designs because they can support deterministic streaming pipelines, where sensor data is processed as it arrives, provided the wider memory, interface, and control architecture is designed to preserve predictable timing. For simpler always-on systems, microcontroller units (MCUs) with integrated sensor interfaces or machine learning (ML) accelerators can enable immediate local inference, while system-level choices such as hardware timestamping, deterministic Ethernet, real-time operating systems, and careful interrupt handling can also directly impact response time.

Hardware and System Design for Latency-Sensitive AI

Latency is not solved by a single component choice alone. It depends on how the entire system is arranged, from the sensor and memory path to the execution model and software stack, making it one of the earliest architectural inputs in latency-sensitive AI design. This is where Avnet Silica’s expansive line card and in-house experts can help engineers evaluate the trade-offs and identify suitable hardware architectures from the outset.

Avnet Silica supports this process by providing access to a broad supplier ecosystem, including AMD, NXP, DEEPX, Renesas, STMicroelectronics, Microchip, onsemi, and Micron. This spans processing platforms, edge AI accelerators, memory and storage, sensors, connectivity, and power management, allowing engineers to consider the full latency path rather than focusing on processor performance alone.

Example Hardware for Real-Time and Latency-Critical AI Systems

DEEPX provides a strong example of where this is heading at the edge. Available through Avnet Silica, the exclusive EMEA distributor, DEEPX AI processors are designed for on-device intelligence, helping to reduce reliance on cloud connectivity where response time, power, and privacy matter. The DX-M1M.2 AI accelerator delivers 25 TOPS in a compact 2280 form factor, integrating 4 GB of high-bandwidth LPDDR5 memory and drawing just 2-5 W under typical inference workloads. Crucially for latency-sensitive designs, the platform prioritises Inferences Per Second (IPS) per watt, supporting applications such as advanced driver assistance systems (ADAS), industrial robots, autonomous mobile robots (AMRs), drones, edge servers, and AIoT devices where every inference must deliver practical value within tight power limits.

DEEPX’s YOLOv7 benchmark data

Figure 1: This level of performance ensures that on-device systems can maintain high-level AI capabilities without compromise

NXP’s i.MX 95 application processor family highlights a different approach, integrating AI acceleration, control, connectivity, safety, and vision processing within a single system-on-chip (SoC) platform. Its eIQ® Neutron neural processing unit (NPU), image signal processing, camera interfaces, high-speed Ethernet, time-sensitive networking (TSN), CAN FD, and real-time control capabilities help reduce the number of external hand-offs between sensing, inference, and system response. This makes it relevant for latency-sensitive applications such as robotics, further supported by NXP’s Robotics Edge Platform, an all-in-one software platform that combines a Yocto-based Robot Operating System (ROS) 2 distribution for i.MX processors with industrial protocols and real-time capabilities to accelerate robotics development at the edge.

Conclusion

As AI moves closer to machines, vehicles, robots, and industrial processes, response time becomes directly linked to safety, reliability, and system performance.

Within these constraints, hardware must be evaluated differently. Raw compute capability remains important, but it cannot be considered in isolation from data movement, memory locality, sensor interfaces, deterministic execution, and the wider system architecture.

As real-time AI applications scale, this perspective becomes increasingly important. Systems that need to perceive, decide, and act within tightly bounded timeframes must be designed around latency from the outset, rather than adjusted late in development.

Latency is therefore a practical way to assess whether an AI system can operate reliably in the real world, and a critical input to choosing the hardware architecture that supports it.

[1] https://www.juniperresearch.com/press/physical-ai-deployments-in-manufacturing-logistics-to-reach-400-000-systems-by-2030/

[2] https://www.strategyand.pwc.com/de/en/industries/telecommunication-media-and-technology/physical-ai.html

Working on a project (LC)

Working on an Artificial Intelligence project?

Our experts bring insights that extend beyond the datasheet, availability and price. The combined experience contained within our network covers thousands of projects across different customers, markets, regions and technologies. We will pull together the right team from our collective expertise to focus on your application, providing valuable ideas and recommendations to improve your product and accelerate its journey from the initial concept out into the world.

WE'D LOVE TO HEAR FROM YOU!

Michael Uyttersprot Author (LC)

About Author

 

Michael Uyttersprot
Michaël Uyttersprot

Michaël Uyttersprot is Avnet Silica's Market Segment Manager for Artificial Intelligence, Machine Learning and Vision. He has 20 years of experience in the industry, starting his career as an engineer in robotics. His current focus is on supporting the development and promotion of embedded vision and deep learning solutions to customers for projects involving AI and machine learning. Michael is seen as a thought leader in the field of AI and ML and has presented his work and thoughts to large audiences at industry events such as Hardware Pioneers Max.

Modal - AI

Contact us

Submit your inquiry via the form below.